Search FAQs
How to install SoMachine Gateway on the new iPC ranges to use SoMachine Protocol
Issue
The Magelis iPC model numbers starting with HMIPSP/HMIPSO (S-Panel PC), HMIPEP (Enclosed Panel PC), HMIBM (Modular Box PC), and HMIRS (Rack PC) are now supported in SoMachine v4.3. How do I install the SoMachine Gateway on them for communication within a SoMachine network of devices?
Product Line
Magelis iPC - S-Panel PC, Enclosed Panel PC, Modular Box PC, Rack PC
Environment
Windows 7, Windows 10
Cause
The new Magelis iPC series starting with HMIPSP, HMIPSO, HMIPEP, HMIBM and HMIRS are newly supported in SoMachine software since version V4.3 and Vijeo Designer v6.2 Service Pack 6.1. These series of Magelis iPCs do not have the SoMachine Gateway pre-installed. Therefore, if you install an old version of Vijeo Designer Runtime on these iPCs and then download your project, the runtime will be updated and the download will be completed successfully. But the communication won’t work because the SoMachine Gateway is not installed on these iPCs.
Resolution
Vijeo Designer Runtime for Windows "v6.2 Service Pack 6.1" (6.2.6.1008):
Attached to this FAQ as: "Vijeo Designer Runtime v6.2.6.1008.zip" (63MB)
Gateway Files for SoMachine v4.3:
Attached to this FAQ as: "Gateway Files for SoMachine v4.3.zip" (89.3MB)
Follow these steps:
The Magelis iPC model numbers starting with HMIPSP/HMIPSO (S-Panel PC), HMIPEP (Enclosed Panel PC), HMIBM (Modular Box PC), and HMIRS (Rack PC) are now supported in SoMachine v4.3. How do I install the SoMachine Gateway on them for communication within a SoMachine network of devices?
Product Line
Magelis iPC - S-Panel PC, Enclosed Panel PC, Modular Box PC, Rack PC
Environment
Windows 7, Windows 10
Cause
The new Magelis iPC series starting with HMIPSP, HMIPSO, HMIPEP, HMIBM and HMIRS are newly supported in SoMachine software since version V4.3 and Vijeo Designer v6.2 Service Pack 6.1. These series of Magelis iPCs do not have the SoMachine Gateway pre-installed. Therefore, if you install an old version of Vijeo Designer Runtime on these iPCs and then download your project, the runtime will be updated and the download will be completed successfully. But the communication won’t work because the SoMachine Gateway is not installed on these iPCs.
Resolution
Vijeo Designer Runtime for Windows "v6.2 Service Pack 6.1" (6.2.6.1008):
Attached to this FAQ as: "Vijeo Designer Runtime v6.2.6.1008.zip" (63MB)
Gateway Files for SoMachine v4.3:
Attached to this FAQ as: "Gateway Files for SoMachine v4.3.zip" (89.3MB)
Follow these steps:
- Ensure that your SoMachine v4.3 configuration software on your PC/Laptop Workstation (not the iPC) is updated with Vijeo Designer v6.2 Service Pack 6.1. You can find this download package from the Schneider Electric Software Update Tool that comes with SoMachine v4.3. It will be named "SoMachine V4.3 Vijeo 6.2.6.1 Update" or from the link above.
- Uninstall any existing Vijeo Designer Runtime from your Magelis iPC.
- Download the Gateway_16.1.0.0_17.05.05.01.zip and GatewayOptionalDrivers_16.1.0.0_17.05.15.01.zip files (attached in "Gateway Files for SoMachine v4.3.zip")
- Install Vijeo Designer Runtime for Windows V6.2 SP6.1 as Administrator
- Download and extract the Gateway_16.1.0.0_17.05.05.01.zip and GatewayOptionalDrivers_16.1.0.0_17.05.15.01.zip files from the link above
- Run the "Gateway_16.1.0.0_17.05.05.01.zip" \installer\setup.exe As Administrator
- Then run the "GatewayOptionalDrivers_16.1.0.0_17.05.15.01.zip" \installer\setup.exe As Administrator
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Category:
Explore more
Range:
Category: