Does RealStream Lift Station allow submersible pump sensors to be connected to it?
The RealStream Lift Station allows the submersible pump sensor relays like temperature and seal failure to be fed directly into the controller, which will automatically stop the pump if configured.
Released for:Schneider Electric Nigeria
Explore more
Range:
RealStream Lift Station
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.