{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What Operating Systems are supported with Telepace Studio 5.2.1 ?
System Requirements

Telepace Studio is supported on these Operating System platforms.

· Windows 8 on 32-bit and 64-bit platforms.

· Windows XP Professional on 32-bit platforms.

· Windows Vista Ultimate on 32-bit and 64-bit platforms.

· Windows Vista Enterprise on 32-bit and 64-bit platforms.

· Windows 7 Professional on 32-bit and 64-bit platforms.

· Windows 7 Ultimate on 32-bit and 64-bit platforms.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: