{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What color are the NetShelter SX pallet brackets?
Issue:
The customer is hoping to use the pallet brackets to mount the cabinet to the floor.

Product Line:
NetShelter SX cabinets

Environment:
All models, all serial numbers.

Cause:
The customer wants to know if the pallet bracket color matches the cabinet color.

Resolution:
The color of the pallet brackets used in the NetShelter SX match the color of the cabinet.

Schneider Electric Nigeria