Search FAQs
How many SCADA clients can be connected to an Easergy T300 using IEC 104 protocol?
- There is a limitation of 8 redundant connections to create multiple SCADA channels using the IEC104 protocol. Create 1 channel per client.
- Make sure to fill-in the Remote IP@ list field. It shall be different for every channel
- Please refer to attached file
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: