{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is the JOG function programmed on the ATV340 drive?
Issue:
How to program the ATV340 drive for JOG?

Product Line:
Altivar 340

Environment:
All

Cause:
N/A

Resolution:
From the main menu, select menus Complete settings -> Generic functions -> Jog.
Default settings as follows.
JOG    Jog assignment, set as appropriate
JGF    Jog frequency,    10 Hz.
JGT    Jog delay,    0.5 s.

See attached file.

Schneider Electric Nigeria

Attachment(s)
ATV340 JOG.pdf [135.48 KB]