{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which slot should the CANOPEN card be installed on an ATV340 with E suffix drive?
Issue:
Slot for canopen card to be installed on an ATV340 with E suffix drive.

Product Line:
Altivar 340

Environment:
All

Cause:
N/A

Resolution:
The ATV340...E version of the drive is strictly for Ethernet IP or Ethernet TCP.  No option modules for communications will work in that drive.

Schneider Electric Nigeria