{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do I need to get an activation code for SoMachine V4.3 OPC UA?

Issue
Is a paid Activation ID or license required for OPC UA in SoMachine v4.3?

Product Line
SoMachine v4.3

Environment
PLC Configuration Software

Resolution
Prior to SoMachine V4.3 Patch 2, an activation code was required to get the OPC UA feature to be licensed and activated.
This activation code was provided through tech support at no additional cost.
With Patch 2 applied to SoMachine v4.3, the OPC UA  no longer requires an activation code.
SoMachine v4.3 Patch 2 is available through the Schneider Electric Software Update tool (SESU).

Note: The current iteration of SoMachine is now EcoStruxure Machine Expert v2.1

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: