{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can the Digital inputs status be monitored on the Altivar Process Drives?

Article available in these languages: Spanish

Issue:
Need to confirm that the Altivar Process drive is recognizing the digital inputs.

Product line:
ATV600, ATV900, Altivar Process

Environment:
n/a

Cause:
Troubleshooting drive

Resolution:
Push the Home button to get to the Main Menu.
From the Main Menu, navigate to Display -> I/O Map -> Digital Input Map.

It will now display the status of the STOA, STOB and Digital Inputs 1 thru 8.  The contact is closed if the Input shows High (or up).  The contact is open if the input shows Low (or down).

Note:  From this menu, highlight and enter each input to check which functions are assigned to it.

Schneider Electric Nigeria