Can I assign IP address on the same subnet on the Magelis HMIG3U using Vijeo Designer V6.2 SP6
No. The IP address for Ethernet 1 and Ethernet 2 on the HMIG3U must be on different subnet with Vijeo Designer V6.2 SP6 or higher.
SR6 release notes
Cannot configure both Ethernet ports on the HMIG3U on the same subnet When defining the IP address for the two Ethernet ports on the HMIG3U target machine, do not configure both Ethernet ports on the same subnet.
Released for:Schneider Electric Nigeria
Explore more
Range:
Harmony GTU
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.