{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Short Circuit Rating of SYBTU1-PLP & SYBTU2-PLP Batteries

Article available in these languages: Spanish

Issue:
Request for the short circuit ratings of the SYBTU1, and SYBTU2 batteries.


Product line:
Symmetra PX, Smart UPS VT


Environment:
All models, all serial numbers


Cause:
Request for information on the short circuit ratings of the battery modules used in the Symmetra PX and Smart UPS VT systems.


Resolution:
The short circuit rating of the battery module is limited by the fuses inside it.  The SYBTU1-PLP, and SYBTU2-PLP battery modules have fuse part #515-1063-Z.
Fuse Fast 63 Amp 500 VDC / 690 VAC ROHS

Bussmann Spec Sheet attached.



Schneider Electric Nigeria

Attachment(s)
Bussmann fuses spec sheet 515-1063_REV02.pdf [49.94 KB]