{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Basic Setup of a M340 BMXNOC0401 module compared with a M580 BMENOC0301 module.
Issue
Comparing Basic Configuration of M340 BMXNOC0401 & M580 BMENOC0301

Product Line
Modicon M580 BMENOC0301 M340 BMXNOC0401

Environment
Unity Pro DTM Browser

Resolution
Below is a video that compares the basic setup of a M340 BMXNOC0401 module with the basic setup of a M580 BMENOC0301 module.

Schneider Electric Nigeria