{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: What is the part number of the cable that connects the expansion modules to main controller for TeSys T?
Issue:
Understanding Connection Cable Options for TeSys T Extension Module

Product Line:
TeSys T, Expansion module LTME

Environment:
Main Controllers and Extension Modules

Cause:
Different cable lengths may be needed for various applications and rail layouts.

Resolution:
3 cable options.
LTMCC004: 0.04m ( 0.13feet).
LU9R03: 0.3m ( 1 foot)
LU9R10: 1m (3 feet)

Schneider Electric Nigeria