Search FAQs
Will TwidoSuite software run on a Windows 10 machine?
Issue:
Can TwidoSuite run on Windows 10 ?
Product Line:
Twido, TwidoSuite
Environment:
TwidoSuite
Cause:
Can't get Twidosuite to run on Windows 10.
Resolution:
No. TwidoSuite, Twido is an obsolete product and has been replaced with the M221 and EcoStruxure Machine Exert Basic ( formally TwidoSuite) software that will run on Windows 10. The last version of TwidoSuite is version 2.31.4 and it will run on Windows 7 64 bit. With the Ecostruxure Machine Expert Basic and M221 you can import the old Twido programs into Machine Expert Basic and load program into the M221.
Can TwidoSuite run on Windows 10 ?
Product Line:
Twido, TwidoSuite
Environment:
TwidoSuite
Cause:
Can't get Twidosuite to run on Windows 10.
Resolution:
No. TwidoSuite, Twido is an obsolete product and has been replaced with the M221 and EcoStruxure Machine Exert Basic ( formally TwidoSuite) software that will run on Windows 10. The last version of TwidoSuite is version 2.31.4 and it will run on Windows 7 64 bit. With the Ecostruxure Machine Expert Basic and M221 you can import the old Twido programs into Machine Expert Basic and load program into the M221.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: