{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Vijeo Designer and EcoStruxure Operator Terminal Expert Runtime have the year 2038 limitation?

Article available in these languages: Spanish

Issue:
On a Mageils HMI running Vijeo Designer or EcoStruxure Operator Terminal Expert, the date can only go as far as December 31, 2038.

Product Line
Magelis HMI ranges, Harmony HMI ranges, Vijeo Designer, EcoStruxure Operator Terminal Expert

Resolution:
Since Vijeo Designer and EcoStruxure Operator Terminal Expert Runtime are currently both 32-Bit applications, they both will be affected by the year 2038 problem. That is, the date and time that the HMI can hold can only be upto the year 2038.

Schneider Electric Nigeria