{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is ISO 9001 or 14001 available for NetShelter SX, SV or CX cabinets?
Issue:
ISO certifications are not noted on the individual product pages of the APC website.

Product Line:
NetShelter SX, SV or CX cabinets and all accessories.

Environment:
All models, all serial numbers.

Cause:
A customer is requesting ISO 9001 and/or 14001 certification for specific NetShelter cabinets or accessories.

Resolution:
An ISO certification (9001 and 14001) is on a company's quality system and environmental system respectively, there is no ISO for an individual product.
Here's a link to the APC by Schneider Electric ISO documents: http://www.apc.com/us/en/who-we-are/sustainability/environmental-compliance/quality-environmental-policies.jsp

Schneider Electric Nigeria