{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Graphic Display terminal VW3A1111 of Altivar Variable speed drives (ATV6xx/ATV9xx) used for RESET function
VW3A1111 Graphic Display terminal can be used for Drives RESET regardless of the Control Channel used, but it needs to be enabled.

This parameter is present in the menu:
5.5 Command and Reference
Stop key Enable (PST parameter)   YES  (by default)
Now  press enter on this parameter, and you will see:
The values:  no - yes - all.

When all is selected, the drive can be reset regardless of control channel.

Schneider Electric Nigeria