{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
PM5340 restarts automatically when trying to configure Modbus, Ethernet or BACnet through meter HMI
PM5340 meter restarts when trying to configure Modbus, Ethernet or BACnet through the meter HMI.
This is known issue and it is fixed in the firmware V2.1.37.

Use DLF3000 tool to upgrade the firmware and Default IP address of the meter is 85.16 as the first two values of the IP address, then convert the last two hexadecimal values of the MAC address to decimal and use this as the last two values of the IP address.

Ex: MAC address =00:80:67:82:B8:C8
Default IP =85.16.184.200

Refer the KB article FA236782 for DLF3000 upgrade procedure

 

Schneider Electric Nigeria

Attachment(s)
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.