{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the "PMESWT0100" a modbus master or a modbus slave?
The weighing module "PMESWT0100" is able to manage an HMI for monitoring / adjustment.
The HMI is connected to the "PMESWT0100" through a RS485 bus. The protocol which is used is Modbus.
The HMI is master on the RS485 bus and the "PMESWT0100"  is slave. We adjust the slave address of the module through the DTM available in the software "UnityPro".

Schneider Electric Nigeria

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: