Search FAQs
What is a SCF3 fault on a ATV320 drive?
Issue:
ATV320 drive showing an SCF3 faultProduct Line:
ATV320
Environment:
SCF3
Cause:
n/a
Resolution:
This is a ground Short Circuit fault.
Recheck all the motor parameters. Check all the cables connecting the drive to the motor, and the motor insulation. Reduce the switching frequency. Check the adjustment of speed loop and/or brake, if applicable. Increase the Time to Restart ( ttr parameter in Set menu) - if there is a brake? Disconnect the motor leads and then turn off the OPL and try to run the drive open circuit and see if it still faults. If it does, the drive appears to be inoperative
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: