Issue
BACnet Support in the PM5300 series.
Product Line
PM5320
PM5340
PM5341
PM5320R
Environment
BACnet Communication
Resolution
The BACnet protocol is implemented only in Ethernet variants of PM53xx series meters. So BACnet MS/TP is not supported in PM53xx series.
PM5320, PM5340 and PM5341 meters do not support BACnet MS/TP (BACNet Serial), these meters support only BACNet IP (over Ethernet)
BACnet Support in the PM5300 series.
Product Line
PM5320
PM5340
PM5341
PM5320R
Environment
BACnet Communication
Resolution
The BACnet protocol is implemented only in Ethernet variants of PM53xx series meters. So BACnet MS/TP is not supported in PM53xx series.
PM5320, PM5340 and PM5341 meters do not support BACnet MS/TP (BACNet Serial), these meters support only BACNet IP (over Ethernet)
Released for:Schneider Electric Nigeria