{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to achieve freewheel stop while controlling the ATV320 drive over profinet protocol?

Article available in these languages: Spanish

Issue:
Activate FreeWheel Stop Over Profinet on an ATV320

Product Line:
Altivar 320.

Environment:
All

Cause:
N/A

Resolution:
On profinet :
Telegram 1 used PROFIDRIVE
Other Telegram use the native drive command (mean I/O profile or CIA402)

CHCF = SIM or SEP :
Send the sequence 0x6, 0x7 and 0xF in order to start.
To stop in freewheel, send 0x0 in CMD

CHCF = I/O:
Write 1 in the bit 0 of CMD to start.
Write 0 bit 0 to stop according STT parameter. So configure STT to Freewheel in order to stop in freewheel.

if this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria