{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Can the faceplate of the ATV320 drive be mounted sideways?

Article available in these languages: Spanish

Issue:
What options do you have when Mounting Altivar 320 Faceplate?

Product Line:
ATV32, ATV320

Environment:
All ATV32 series, ATV320 "B" type only.

Cause:
Application requires horizontal mounting for control access.

Resolution:
The faceplate of the Bookshelf Version of the ATV320 can be mounted Horizontally.  This only applies to the drives with part number ATV320..B.  It will require a modification of the drive, and an additional mounting bracket will be needed.  The part number for this bracket is VW3A9920.

Schneider Electric Nigeria