{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it mandatory to perform EMC tests ?
According to IEC 6221-100 table 11, EMC (Electromagnetic Compatibility) tests are mandatory only if electronic equipment or components are included in the secondary system.

IEC 62271-1 "common specification for HV switchgear and controlgear", § 7.9.1.2 and 7.9.2.1 specifies
"Auxiliary and control circuits of switchgear and controlgear shall be subjected to electromagnetic emission tests or electromagnetic emission tests if they include electronic equipment or components.
In other cases no tests are required".

Therefore these tests concern mainly Evolis 17.5 kV which uses releases (UVR, opening, closing) with electronic component inside.

Schneider Electric Nigeria