Search FAQs
Galaxy VX; Customer, consultant or engineer looking for the center of gravity (CoG) for the IO and/or PC enclosures
Issue:
Customer, consultant or engineer looking for the Center of Gravity (CoG) for the IO and/or PC enclosures.
Product line:
Galaxy VX
Environment:
All models, all serial numbers
Cause:
none.
Resolution:
The enclosures have the following CoG.
- GVX PC: X-distance 290mm, Y-distance 930mm , Z-distance 440mm
- GVX 750kW IOC: X-distance 590mm, Y-distance 830mm, Z-distance 390mm
- GVX 1000kW IOC: X-distance 590mm, Y-distance 830mm, Z-distance 390mm
- GVX 1500kW IOC: X-distance 1060mm, Y-distance 970mm, Z-distance 430mm
- GVXMBCR750: X-distance 399.7mm, Y-distance 993mm, Z-distance 471.5mm
(X=width, Y=height, Z=depth)
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: