{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV process, does FDR works towards new fw version?
We can confirm that latest Ethernet channel evolution's have brought FDR service improvements.
With todays fw versions :
ATV6xx:  version 2.2ie24 (internally, the embedded Ethernet firmware version must be 1.Die15)
ATV9xx: version 1.8ie14 (internally, the embedded Ethernet firmware version must be 1.Die15)
Eth.card VW3A3720: version 1.Die15
or any newer version, the FDR will work towards equal or newer fw version.

Example1: today ATV2.2IE24 is used and after one year it will be replaced by ATV with newer fw (e.g. 2.3IExx). Result is that FDR OK
Example2 : ATV1.9IE24 has been used and now it is going to be replaced by ATV 2.2IE24. Result is that FDR is not OK.

Schneider Electric Nigeria