{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the installation requirements for Citect SCADA 2018?

Issue

What are the the software and hardware requirements for Citect SCADA 2018?

Product Line

Citect SCADA

Environment

Windows 7, Windows 10, Windows Server 2012 R2

Resolution

Please see the attached <<Installation Guide.pdf>> starting in Chapter 4 (page 44).

Note that Hardware requirements (CPU) vary depending on the number of the number of I/O per server.
Use the tables starting on page 44 to identify the CPU Benchmark (PassMark) score required.
You can then cross-reference the score with eligible CPUs from a website which reports on tested CPU performance such as https://www.cpubenchmark.net/

Also note that the domain "citect.schneider-electric.com" will redirect you to AVEVA -  the brand under Schneider Electric that makes Citect.
For support on all AVEVA products including Citect, go to: https://softwaresupport.aveva.com/

Schneider Electric Nigeria

Attachment(s)
Installation Guide.pdf [2.37 MB]