{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can Magelis HMI communicate with an Allen-Bradley CompactLogix 5370 PLC via 1769-L30ER?

Issue

I would like to read and write from my Magelis HMI to an Allen-Bradley CompactLogix 5370 PLC via 1769-L30ER module.

Product Line

Vijeo Designer, Magelis HMI (XBTGT, XBTGK, XBTGH, HMISTU, HMISCU, HMIGTO, HMIGTU)

Resolution

For the Magelis HMI to communicate to an Allen-Bradley CompactLogix 5370 PLC via 1769-L30ER module, use the Allen-Bradley Ethernet/IP
In the Vijeo Designer configuration software, the protocol can be added under the IO Manager node in the Navigator pane.
Driver selection

From the CompactLogix software, one can export an .L5K file and Link Variables to Vijeo Designer in order to sync the tags.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: