{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the PM5000, PM8000, ION7650, ION8650 and ION9000 meters calibrated to ANSI C12.20 at unity power factor?
Product Line
PM5000, PM8000, ION7650, ION8650 and ION9000

Environment
Meter Specifications

Resolution
Schneider Electric does not calibrate to C12.20, we verify to it.  The ANSI C12.20 claim is as follows:

ION9000/ION8650 Accuracy Class 0.1 (0.1% energy accuracy at unity PF)
PM5000/PM8000/ION7650 Accuracy Class 0.2 (0.2% energy accuracy at unity PF)

Schneider Electric Nigeria