{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What types of cables are compatible with the Compact NSX bare cable connectors?
The Compact NSX bare cable connectors (reference numbers listed in the attachment) can be used with solid or stranded cables.

Stranded cables, with cross sections indicated in the connectors instruction sheet, may be used without cable ends (ferrules). In case cable ends (ferrules) are used, it is advised to consider the maximum cross section compatible one size smaller than indicated in the instruction sheet. The cable end is increasing the diameter of the cable inserted in the connector.

Schneider Electric Nigeria

Attachment(s)
bare cable connectors NSX400-630.JPG.jpg [32.41 KB]
bare cable connectors NSX100-250.JPG.jpg [74.59 KB]