{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the minimum peripheral module firmware requirements for M580 Hot Standby?

Article available in these languages: Spanish

Below are the required minimum firmware versions in order to be compatible with a redundant M580 PAC.
ReferenceDescriptionMinimum Firmware Version
BMXCRA31200X80 Standard Drop Adapter2.14
BMXCRA31210X80 Performance Drop Adapter2.14
BMECRA31210X80 Performance Drop e-Adapter2.14
140CRA31200**Quantum Ethernet Drop Adapter2.14
BMENOC0301M580 Ethernet Scanner2.04
BMENOC0311M580 FactoryCast Ethernet Scanner2.04

Note: Though matching revisions is recommended, as long as the above minimum requirements are met, mixing versions is allowed. 
** Quantum drops are not supported with the BMEH582040.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria