{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do I add a remote drop to an M580 configuration?
Issue
Procedure to adding a remote drop to an M580 configuration in Unity Pro.

Product Line
Modicon M580 ePAC (Ethernet Programmable Automation Controller)

Environment
Unity Pro

Resolution
To add a remote drop to an M580 configuration, you need to open the EIO bus. Once the EIO bus is open you can double-click the small box. That will launch a window where you can select the appropriate rack and CRA.

Note: There is a similar small box directly under the local rack in PLC bus window. Double-clicking this box does NOT add a remote drop but rather an extended rack.

Schneider Electric Nigeria