{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the AR9000RAMP be used on the shock pallet of the AR3xxxSP cabinets?
Issue:
A customer may want a reusable ramp to use on AR3xxxSP cabinets.

Product Line:
NetShelter SX SP, SX3K

Environment:
All versions and serial ranges.

Cause:
If a customer looses their shock packaging ramp, or requests a reusable ramp, is there one available for the AR3xxxSP cabinets?

Resolution:

The NetShelter shock packaging (AR3xxxSP) cabinets ship with single use wooden ramps.
The NetShelter SX3K Integrator Ready (AR9xxx) cabinets have a reusable metal ramp available with with the cabinet, or separately under sku AR9000RAMP.
The AR9000RAMP is also compatible with the NetShelter SX shock packaging cabinets (AR3xxxSP)

Schneider Electric Nigeria