{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to Migrate a Framework(Template) from an ION7x50 to ION9000?
Issue
Uploading an ION7x50 template file directly to ION9000 does not allow the ION9000 to function correctly.

Product Line
ION7x50
ION9000

Environment
Framework

Cause
Due to the structural changes on some modules and modifications on the new platform, the use of some modules on the default framework of the ION9000 meter may differ from the default framework on the ION7x50 meters.

Resolution
Please see the attached document.

Schneider Electric Nigeria

Attachment(s)
Custom Framework Migration_V1.2.docx [1.23 MB]