Issue:
Sleep functionality on ATV320.
Product Line:
Altivar 320
Environment:
All
Cause:
Needs sleep function for application
Resolution:
The ATV320 doesn't have a sleep parameter, but a sleep functionality can be accomplished by using the tLS and rSL parameters when running PID.
tLS (Low speed time out) is adjustable from 0 to 999.9 seconds, and defines the amount of time the drive can run at low speed before an automatic stop is requested.
rSL (PID wake up threshold) can be used to set the PID error threshold above which the PID regulator will be reactivated (wake-up) after a stop due to the max. time threshold being exceeded allow speed [Low speed time out] (tLS).
See the ATV320 Programming Manual for further details:
https://www.se.com/us/en/download/document/NVE41295/
Sleep functionality on ATV320.
Product Line:
Altivar 320
Environment:
All
Cause:
Needs sleep function for application
Resolution:
The ATV320 doesn't have a sleep parameter, but a sleep functionality can be accomplished by using the tLS and rSL parameters when running PID.
tLS (Low speed time out) is adjustable from 0 to 999.9 seconds, and defines the amount of time the drive can run at low speed before an automatic stop is requested.
rSL (PID wake up threshold) can be used to set the PID error threshold above which the PID regulator will be reactivated (wake-up) after a stop due to the max. time threshold being exceeded allow speed [Low speed time out] (tLS).
See the ATV320 Programming Manual for further details:
https://www.se.com/us/en/download/document/NVE41295/
Released for:Schneider Electric Nigeria