{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Buildtime License do I need if I want to have multiple EcoStruxure Machine SCADA Expert (Vijeo XL) Runtimes supporting 4k Tags?
Issue

If I have 12 iPC devices running EcoStruxure Machine SCADA Expert with the 4000 Tags License (HMIVXLRT4KLV80), do I need to have my Buildtime software support at least 12*4000=48,000 Tags?

Product Line

EcoStruxure Machine SCADA Expert, Vijeo XL

Environment

Windows 7, Windows 10

Resolution
No. A Buildtime License supporting 4000 Tags will suffice because a single project will have the maximum of 4000 tags.
If you have 12 iPCs with Runtime, each of those individual projects only have a maximum of 4000 tags.

Part Numbers for the Buildtime softfware are:

HMIVXLBT4KL80

EcoStruxure Machine SCADA Expert (Vijeo XL) with 4000 tags

HMIVXLBT4KDV80

EcoStruxure Machine SCADA Expert (Vijeo XL) with 4000 tags plus DVD

For other licenses requiring a different number of tags, replace the '4K' with:

1K’ for 1500 tags

32K’ for 32,000 tags

64K’ for 64,000 tags


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria