{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I add the Magelis HMIGXO in Vijeo Designer?

Issue
The Magelis HMIGXO series are only available for the APAC Market. However, sometimes a machine built by an overseas machine builder may sell and deliver a machine to a customer in another part of the world and it might be necessary to update the application with Vijeo Designer if the equipment was shipped to a different country,

Product Line:
HMIGXO3501
HMIGXO3502
HMIGXO5502

Environment
Vijeo Designer V6.2 Standalone version only.
Does not apply to Vijeo Designer installed under SoMachine or EcoStruxure Machine Expert

Resolution

To give access to programming the GXO target in Vijeo Designer V6.2
1. Launch Vijeo Designer as Administrator in Windows.
2. Go to Help->About->License->Upgrade.
3. Enter the Upgrade Reference Number VJDHTGTGX and press OK.
4. Close Vijeo Designer.
5. Relaunch Vijeo Designer.

Note: Vijeo Designer must be registered before the upgrade can be applied.

Schneider Electric Nigeria