Issue:
Is it possible to Export SoMove file for AC Drive and Soft starter.
Product Line:
Altivar AC Drive, Soft starter
Environment:
All
Cause:
Customer wanted to save SoMove file of the ATV320 in PDF file.
Resolution:
In SoMove,
1) Click on File on the Menu Bar
2) Scroll down to Export and select "Export to PDF file"
(Note: Can also Export to .XLS or .TXT file)
3) Create a file name for your PDF file in the Save As Window
4) Click Save to save PDF file in your folder
Released for:Schneider Electric Nigeria