{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I download Vijeo Designer v6.2 Service Pack 6?
Issue
Where can I download Vijeo Designer v6.2 Service Pack 6?
The version numbers are as follows:
Editor/Buildtime: 6.2.6.39
Runtime: 6.2.6.39

Product Line
Vijeo Designer v6.2

Resolution
Vijeo Designer V6.2 SP6 install files (Updated 2023-02-21) are attached to this FAQ.

1) Just the patch to install on top of the existing Vijeo Designer v6.2 installed on your PC/laptop for the Development Environment (341MB):
"Vijeo_Designer_Development_SP6(6.2.6.39_6.2.6.39).zip"

2) Help files update to your Vijeo Designer v6.2 (Vijeo Designer HTML help files and PDF manuals) - 1129MB:
"SP6_Docs_Pack(6.2.6.39_6.2.6.39).zip"

3) iPC/Standard PC Runtime if you need to have an iPC/Standard PC running as an HMI by itself - 64MB:
"Runtime_For_Windows_SP6(6.2.6.39_6.2.6.39).zip"

4) Data Manager for retrieving Logging/Recipe data from an HMI (this is installed on your laptop/PC on top of your existing Vijeo Designer v6.2) - 61MB:
"DataManager_SP6(6.2.6.39_6.2.6.39).zip"

5) Web Gate Client Files (this is for if you are connecting to the HMI and want to mirror the screen on a remote PC's browser) - 19MB:
"Web_Gate_Client_Files_SP6(6.2.6.39_6.2.6.39).zip"

Schneider Electric Nigeria

Attachment(s)
Vijeo_Designer_Development_SP6(6.2.6.39_6.2.6.39).zip [332.9 MB]
Runtime_For_Windows_SP6(6.2.6.39_6.2.6.39).zip [62.91 MB]
SP6_Docs_Pack(6.2.6.39_6.2.6.39).zip [1.08 GB]
DataManager_SP6(6.2.6.39_6.2.6.39).zip [59.62 MB]
Web_Gate_Client_Files_SP6(6.2.6.39_6.2.6.39).zip [18.93 MB]