Search FAQs
What are the Part Numbers for the touch screen attachments for the Harmony/Magelis HMIS5T or HMISCU?
Issue
What are the Part Numbers for the touch screen attachments for the Harmony/Magelis HMIS5T or HMISCU?
Product Line
Harmony/Magelis HMIS5T
Harmony/Magelis HMISCU
Resolution
The touchscreen front attachment part of the Harmony/Magelis HMIS5T or HMISCU has two sizes, a 3.5 inch touch display and a 5.7 inch touch display - each with the choice of with or without the Schneider Electric logo. All of them have the same mounting solution and cutout hole size and are 320x240 pixels.
All of the following screen modules can be used for Harmony/Magelis HMIS5T and HMISCU processor back modules:
3.5" with Schneider Electric logo:
HMIS65
3.5" without logo:
HMIS65W
5.7" with Schneider Electric logo:
HMIS85
5.7" without logo:
HMIS85W
What are the Part Numbers for the touch screen attachments for the Harmony/Magelis HMIS5T or HMISCU?
Product Line
Harmony/Magelis HMIS5T
Harmony/Magelis HMISCU
Resolution
The touchscreen front attachment part of the Harmony/Magelis HMIS5T or HMISCU has two sizes, a 3.5 inch touch display and a 5.7 inch touch display - each with the choice of with or without the Schneider Electric logo. All of them have the same mounting solution and cutout hole size and are 320x240 pixels.
All of the following screen modules can be used for Harmony/Magelis HMIS5T and HMISCU processor back modules:
3.5" with Schneider Electric logo:
HMIS65
3.5" without logo:
HMIS65W
5.7" with Schneider Electric logo:
HMIS85
5.7" without logo:
HMIS85W
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: