{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does M580 NOP system comply to IEC255-5
Question:
Does M580 NOP system comply to IEC 255-5?

Answer:
IEC255-5 is for EMC standard to withstand impulse input test at its AC input
A M580 PLC rack supplied by a PS module BMXCPS4002 will comply to this requirement.

Schneider Electric Nigeria