Search FAQs
PME Maintenance: How to use PowerShell to stop/Start all ION services
How to use PowerShell to stop/Start all ION services
Issue: How to turn all PME services off and on
Product Line:
Power Monitoring Expert 9.0
Power Monitoring Expert 2023
Environment:
Windows Services
Windows Powershell
Resolution:
When performing PME maintenance or doing some testing, might be required to start/ stop all ION services.
You can use the scripts in attachment to do this task faster.
The scripts will start/stop the following services in this order. -you can edit it if you might require changes-
To stop the services use this command: powershell -command .\Services_Stop.ps1
Note: The scripts are intended to be used with PME9.0, for older versions you will need to edit them to remove the services that do not exist in older versions. Also attached are the PME 2023 version of the scripts.
Issue: How to turn all PME services off and on
Product Line:
Power Monitoring Expert 9.0
Power Monitoring Expert 2023
Environment:
Windows Services
Windows Powershell
Resolution:
When performing PME maintenance or doing some testing, might be required to start/ stop all ION services.
You can use the scripts in attachment to do this task faster.
The scripts will start/stop the following services in this order. -you can edit it if you might require changes-
- W3SVC
- PMLNetman
- IONEW
- PMLLogServer
- PMLION
- IONRS
- PMLSS
- PMLVIP
- PMLXMLSubscriptions
- PMLXMLSubscriptionStore
- PMLMK
- PMLCM
- CoreServicesHost
- DataServicesHost
- ProviderEngineHost
- ManagedCircuitService
- PowerCloudAgentService
- IONDiagnosticsAndUsage
- PMLOGROUTER
- PMALARM
- PMLVIP_VIP.DDD
- PMLVIP_VIP.DEFAULT
- PMLVIP_VIP.PQADVISOR
To stop the services use this command: powershell -command .\Services_Stop.ps1
Note: The scripts are intended to be used with PME9.0, for older versions you will need to edit them to remove the services that do not exist in older versions. Also attached are the PME 2023 version of the scripts.
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Category:
Explore more
Range:
Category: