Search FAQs
How to select the proper fuse rated current for my transformer protection by RM6 switch-fuse unit?
Below selection table gives the fuse rated current based on network (service) voltage and transformer rated power:
Important notes:
Important notes:
- Correct operation of the RM6 is not guaranteed when using fuses from other manufacturers,
- Fuse rating given in A, no overload, – 25°C < Temperature < 40°C),
- Fuse type considers: Fusarc CF and SIBA (1) (General case, IEC 60282-1 standard, IEC 62271-105 (to replace IEC 60420) and DIN 43625 standard),
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: