{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you set up the ATV630 and ATV930 open type drives for damper control?
Issue:
ATV630 and ATV930 drive for damper control.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Damper control option

Resolution:
Damper Control in Altivar Process ATV630

The Altivar Process 600 drives were not designed specifically for HVAC applications in the way
the Altivar 212 drives were, and do not include dedicated ‘Damper Control’ functions. You can,
however, use the ‘Priming Pump’ control function to  control a damper in a similar way.

Use ‘Priming Pump Assignment’ (PPoA) to select the output relay to send the open/close
command.

Use ‘Primed Switch Assign’ (PPWA) to set the logic input for the damper position feedback
input.

Use ‘Priming Time’ (PPSd) to set the delay time from sending a damper open command to the
drive starting the fan rotation.

This does not provide quite the same level of interlocks and error detection that is in the
ATV212 functions, but does allow basic damper control within the drive.

This does not apply to the ATV930 drive which does not have any options for Damper control.


Schneider Electric Nigeria

Can you set up the ATV630 and ATV930 open type drives for damper control?
Issue:
ATV630 and ATV930 drive for damper control.

Product Line:
ATV630 and ATV930

Environment:
All 

Cause:
Damper control option 

Resolution:
Damper Control in Altivar Process ATV630

The Altivar Process 600 drives were not designed specifically for HVAC applications in the way 
the Altivar 212 drives were, and do not include dedicated ‘Damper Control’ functions. You can, 
however, use the ‘Priming Pump’ control function to  control a damper in a similar way.

Use ‘Priming Pump Assignment’ (PPoA) to select the output relay to send the open/close 
command.

Use ‘Primed Switch Assign’ (PPWA) to set the logic input for the damper position feedback 
input.

Use ‘Priming Time’ (PPSd) to set the delay time from sending a damper open command to the 
drive starting the fan rotation.

This does not provide quite the same level of interlocks and error detection that is in the 
ATV212 functions, but does allow basic damper control within the drive.

This does not apply to the ATV930 drive which does not have any options for Damper control. 


 

Schneider Electric Nigeria

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: