{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How does the Fast Stop work on the Altivar 320 drives?
Issue:
How does the Ramp Divider (DCF) affect the deceleration time when the Fast Stop function is used on the AT320 drives?

Product Line:
Altivar 320 ATV320 MACHINE drive

Resolution:
How to figure the resulting ramp time. When using the Fast stop assignment to a logic input (FST = LIx) or as the Type of Stop (STT = FST), the Ramp divider (DCF) affects the normal DEC setting:Fast stop ramp time = DEC divided by DCFDCF is adjustable from 0 to 10Examples:If DEC = 20sec and DCF = 2, then the fast stop ramp is 20 / 2 = 10secIf DEC = 20sec and DCF = 4, then the fast stop ramp is 20 / 4 = 5sec

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.