{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the conduit kits for the ATV630 and ATV930 drives?
Issue:
Conduit entrance kits for ATV630 drives.

Product Line:
Altivar Process

Environment:
Conduit Entrance kits

Cause:
n/a

Resolution:
For both ATV630 and ATV930 drives:
Frame Sizes 1-4 are supplied with the conduit kit already installed on the drives.
Frame size 5 drive are supplied with the conduit kit, but it does not come installed on the drive.
Frame size 6 drive is not supplied with the conduit kit.  Order separately, part number is VW3A9704.
Frame size 7 drive is not supplied with the conduit kit it, needs to be ordered separately.
***The part numbers are for frame size 7A (C22N4 drives) you need VW3A9212 and for frame size 7B (C25N4 and C31N4) you need VW3A9213.

See attachment for reference:



Schneider Electric Nigeria

Attachment(s)
ATV630 Conduit Entrance Kits.png [107.69 KB]