{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is undercurrent fault setup on the Tesys T?
Issue:
Undercurrent fault setup  on the Tesys T.

Product Line:
Tesys T

Environment:
North America

Cause:
Undercurrent fault

Resolution:
Under Parameter List, Current submenu, set undercurrent fault to enable (deactivate is default).
Undercurrent fault threshold min 30% of FLC (Full load current) to 100% FLC.  Default is 50%.
Undercurrent fault timeout has a range of 1 to 200s with default timeout period of 10s.
Undercurrent warning activate allows undercurrent warning threshold to be programmed.  30 to 100%FLC as range and 50% FLC as default.

Schneider Electric Nigeria