Recommended cable cross-section for the Output dv/dt filters used for Frequency inverters Altivar
Information about max cable cross-section that can be connected to output dv/dt filer is published in product datasheet of dv/dt filter. See example in attached picture,
Released for:Schneider Electric Nigeria
Attachment(s)
dv-dt cable cross-section.jpg [260.31 KB]
Explore more
Range:
Altivar Process ATV600
Altivar Process ATV900
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.