{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to use Ethernet IP and Ethernet TCP on the same network using an ATV630?
Issue:
Usage of Ethernet IP option and the integrated Ethernet TCP on the same network with an ATV630

Product Line:
Altivar 630

Environment:
All serial numbers

Cause:
I have several ATV630 monitoring Ethernet, some have option Ethernet cards and some do not.

Resolution
Ethernet IP and Ethernet TCP cannot be used on the same network.

Schneider Electric Nigeria