{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the process to order an 18 pulse Altivar ATV630 or ATV930 Process drive?
Issue
Process to order an 18 pulse Altivar ATV630 or ATV930.

Product Line:
ATV960, ATV630 ATV930 drives

Environment:
18 pulse process drive only

Cause:
Custom ordered drive

Resolution
If you need to order the new Process drive with 18 pulse technology you will need to start with the ATV960 custom drive then choose between 50HP and 500HP.    Now choose 18 pulse EP418 under the Harmonics Migration/Line reactor option.

Schneider Electric Nigeria